Technical FAQs

Ask a Question

Why is Altivar ATV66 getting a random stop command while running?

If it is an older keypad display and there is a noisy power supply than an erroneous stop command on the keypad may occur, especially if there is a jumper from +24 to LI1 and LI2. The keypad can be replaced if this is occurring.

CTA-ID : 6734
Was this helpful?
What can we do to improve the information ?