Technical FAQs

Ask a Question

Can the IGBT output semi-conductor devices be damaged when the motor is disconnected while the Altivar ATV66 drive is running?

Current spikes can be seen at the output of an ATV66 if the motor is disconnected when the drive is running, this can stress the IGBT`s and shorten their life.


CTA-ID : 6920
Was this helpful?
What can we do to improve the information ?