Technical FAQs

Ask a Question

What is the terminal lug data for a C2M200S Combination Service Entrance Device?

The main phase and neutral lugs accept a #4 AWG - 250 KCMIL copper or aluminum conductor. The main service ground lug accepts a #6 AWG - #2/0 AWG copper or aluminum conductor.


CTA-ID : 2027942
Was this helpful?
What can we do to improve the information ?