Technical FAQs

Ask a Question

Why do some Homeline breakers have slotted screw terminals and some have square/slotted terminal screws?

Effective April 4, 2006, 1-pole Homeline 15A and 20A (HOM115 HOM120) breakers began shipping with the combination slot/square-drive terminal screw.


CTA-ID : 2027924
Was this helpful?
What can we do to improve the information ?