Technical FAQs

Ask a Question

Why do some QO breakers have slotted screw terminals and some have square/slotted terminal screws?

Effective April 4, 2006, 1-pole QO 15A and 20A plug-on and bolt-on breakers began shipping with the combination slot/square-drive terminal screw.


CTA-ID : 2027923
Was this helpful?
What can we do to improve the information ?