Technical FAQs

Ask a Question

What is the thread size of a 9049ER12 ?

The Rod is .187 (3/16``) in diameter. Threading is #10-32 for 3/8`` on each end.


CTA-ID : 2027921
Was this helpful?
What can we do to improve the information ?