Technical FAQs

Ask a Question

What is the amount of heat emitted by the QO-AFI circuit breaker? <br />

Watts-loss for the QO120AFI is approximately 3.5 Watts at 80% load.
Watts-loss for the QO115AFI is approximately 2.6 Watts at 80% load.


CTA-ID : 2027905
Was this helpful?
What can we do to improve the information ?