Technical FAQs

Ask a Question

What is the difference between a 9050JCK2* and 9050JCK4* series B and series D?

When we changed manufacturers they eliminated the jumper where before intiating contacts were 5 and 6 or 7. Now, only pins 5 and 6 are used for intiating contacts on standard 9050 JCK off-delay and one-shot . Only pins 5 and 7 are used for intiating contacts on standard 9050 JCK off-delay and one-shot with power trigger (9050JCK**PT ).


CTA-ID : 2027903
Was this helpful?
What can we do to improve the information ?