Technical FAQs

Ask a Question

Why does the AM1DL201 mounting rail have to be used with the AK5PA___ mounting plate tap-off when used on the AK5JB___ panel bus system?

The AM1DL201 mounting rail carries all the weight of all the mounting plate tap-off units, the starters, and the contactors. This is to prevent all the weight from resting on the AK5JK143 panel bus system.


CTA-ID : 2027900
Was this helpful?
What can we do to improve the information ?