Technical FAQs

Ask a Question

Do we have a 600 volt rated 100 amp 3 pole DIN rail mounted circuit breaker?

Issue:

Do we have a 600 volt rated 100 amp 3 pole  DIN rail mounted circuit breaker?

 

Product Line:

Powerpact

 

Environment:

Products sold in North America

 

Cause:

Need a 600V breaker for DIN rail application.

 

Resolution:

Yes, use HDL36100 (or HGL, HJL, HLL) and S29305 DIN rail mounting kit.

Powerpact H & J frame 3-pole breakers can be DIN rail mounted. Use kit # S29305.
DIN rail mounting kit (requires 15 mm depth on a 35 mm DIN rail)
Fits 3 pole module breakers only. (Not available in 2 pole)

See instruction bulletin, 48940-239-01.

CTA-ID : 2027597

Was this helpful?
What can we do to improve the information ?