Technical FAQs

Ask a Question

Is the width dimension of a H328N dimension the same with or without the handle?

Yes, the operating handle is mounted on front of device.


CTA-ID : 2027594
Was this helpful?
What can we do to improve the information ?