Technical FAQs

Ask a Question

What main breakers are provided in a CU12L400CN, CU12L400FN, CU12L400CB, CU12L400FB, QU12L400SL, QU12L400CL or QU12L400FL 400A CSED Meter-Main?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarification

Resolution:
These 400A CSED Meter-Main panels are provided with one QDL22200 main breaker factory installed. Additional space is provided for the field installation of a second QDL main breaker, 200A maximum. Further additional space is provided for the field installation of up to four QOH main breakers, 125A maximum. The total ampacity of the combination of QOH breakers cannot exceed 200A. All of the breakers installed would be considered service disconnects.


CTA-ID : 2027196
Was this helpful?
What can we do to improve the information ?