Technical FAQs

Ask a Question

What is the terminal lug data for a C125RB Combination Service Entrance Device?

The main phase, neutral and service ground lugs accept a #8 AWG - #1/0 AWG copper or #6 AWG - #1/0 AWG aluminum conductor.


CTA-ID : 2027890
Was this helpful?
What can we do to improve the information ?