Technical FAQs

Ask a Question

What main breakers are provided in a CU816D400D400CN, CU816D400CB, QU816D400SL, QU816D400CK, QU816D400CL, QU816D400CLX and QU816D400FL 400A CSED Meter-Main panels?

Issue:
Product Features

Product Line:
CSED

Cause:
Clarification

Resolution:
These 400A CSED Meter-Mains are provided with one QDL22200 factory installed. The factory installed QDL22200 feeds the 8 space/16 circuit loadcenter interior section. Additional space is provided for the field installation of a second QDL main breaker, 200A maximum to feed a downstream sub panel.


CTA-ID : 2027190
Was this helpful?
What can we do to improve the information ?