Technical FAQs

Ask a Question

What is the purpose of a sway brace collar?

Sway braces are used when one side of the busway is more heavily loaded with tap-off units than the other causing the busway to not hang level. The Sway Brace Collar should also be used when other factors could cause possible swaying of the busway.


CTA-ID : 2027561
Was this helpful?
What can we do to improve the information ?