Technical FAQs

Ask a Question

Is the HCR-U interior an I-Line panel?<br /><br />

Yes, this is a new I-line panelboard that superseded the HCWM-U. See Digest 173 page 8-23.


CTA-ID : 2027179
Was this helpful?
What can we do to improve the information ?