Technical FAQs

Ask a Question

What main breakers are used in a RU3040D400CLX?

One QDL22200 is supplied factory installed. The factory installed QDL22200 feeds the 30 space/40 circuit loadcenter interior. Additional space is provided for the field installation of a second QDL main breaker, 200A maximum.


CTA-ID : 2027174
Was this helpful?
What can we do to improve the information ?