Technical FAQs

Ask a Question

Do the protective relay functions of Micrologic trip units meet the ANSI C37.90 relay requirements? Is it certified?

The relay functions meet the ANSI C37.90 relay standard except for the 30A contact output requirement.

This means that the protective relay functions can`t be certified to ANSI C37.90 standards but functionally work the same except they have a 5 Amp output.

CTA-ID : 2027562
Was this helpful?
What can we do to improve the information ?