Technical FAQs

Ask a Question

What is the voltage rating of an XCSE safety interlock switch ?

This switch is rated to handle up to 300vac or dc ....AC-15 , B300 and DC-13 Q300 The solenoid operates at 24 volts, which is supplied by an internal converter when other solenoid operating voltages are specified.


CTA-ID : 2027558
Was this helpful?
What can we do to improve the information ?