Technical FAQs

Ask a Question

Is the QC12L200C supplied with a neutral bonding screw?

This CSED (Combination Service Entrance Device) is not supplied with a neutral bonding screw. CSEDs are UL listed for, and marked as, ``Suitable Only For Use As Service Equipment``. The neutral is factory bonded to the enclosure as a standard feature.


CTA-ID : 2027322
Was this helpful?
What can we do to improve the information ?