Technical FAQs

Ask a Question

What is the % Z , impedance value of the built in line reactor on the new extended range of Altivar ATV58 drives.

ATV58 TRX drive controllers ATV58HD28N4 to ATV58HD79N4 and ATV58HD16M2 to ATV58HD46M2 have built-in line reactors.
The built in line reactor is about 1.5% reactor. This reactor is internal and designed to allow the drive to meet or exceed the specifications for the drive. Additional external line reactors may be installed if necessary.


CTA-ID : 6881
Was this helpful?
What can we do to improve the information ?