Technical FAQs

Ask a Question

What is the difference between the QOUMF1 and the QOUMFS1

The QOUMF1 is the standard mounting foot that comes with the QOU breaker. The QOUMFS1 is similar mounting foot except it has a tapped hole to enable the foot to be secured by a bolt from the front to hold the breaker flush to a panel.


CTA-ID : 2027545
Was this helpful?
What can we do to improve the information ?