Technical FAQs

Ask a Question

What is the current rating for an XUX0ARCTT16 ?<br />

The load current capacity is 3 amps maximum into a pure resistive load (Cosine Theta = 1.0). De-rating is necessary for inductive loads.





CTA-ID : 2027540
Was this helpful?
What can we do to improve the information ?