Technical FAQs

Ask a Question

What are the repair parts for a C1220QRF Combination Service Entrance Device?

Repair Parts

Product Line:
CSED - Obsolete Design


The only replacement part available for this obsolete device would be the main breaker. 
The original main breaker was a Q12100, which is obsolete and no longer available. The Q12100 can be replaced with a QO2100. The QO2100 is smaller that the Q12100, so this change will provide two extra space in load center

CTA-ID : 2027528
Was this helpful?
What can we do to improve the information ?