Technical FAQs

Ask a Question

What amperage is the standard aux. contact used on a Powerpact H frame breaker?

240/380 Vac 6 A
480 Vac 6 A
600/690 Vac 6 A
24/48 Vdc 2.5 A
240 Vdc 0.5 A
380 Vdc 0.3 A



CTA-ID : 2027518
Was this helpful?
What can we do to improve the information ?