Technical FAQs

Ask a Question

Are the Square D Combination Service Entrance Devices built in accordance with the standard UL414?

Product design

Product line:
 Combination Service Entrance Devices

UL Standards 

Meter socket design

The Overall CSED Devices are UL listed in accordance with UL 67 Standard for Panelboards. But the meter socket itself used within the CSEDs is designed and tested in accordance with standards outlined in UL414.

CTA-ID : 2027475
Was this helpful?
What can we do to improve the information ?