Technical FAQs

Ask a Question

What is the temperature rating for the 9007AF and 9007AW limit switches?

Issue:
Product Characteristics

Product Line:
Limit switches

Environment:


Cause:
Temperature rating is an important factor for devices intended for industrial applications where ambient may be well above or below a moderate range of values.

Resolution:
Lever Type: -65 degree F (-54 degree C) to 185 degree F (85 degree C)
Plunger Type: 0 degree F (-17.8 degree C) to 185 degree F (85 degree C)


 
Was this helpful?
What can we do to improve the information ?