Technical FAQs

Ask a Question

Can 9001K2L no guard illuminated pushbutton be converted to full guard.

Issue:
Clarifying if a 9001K2L no guard illuminated pushbutton be converted to full guard.

Product Line:
9001K Heavy Duty operators 30mm Push Button

Environment:
30mm Illuminated Momentary Push Button Operators

Cause:
Determine if a no guard operator can be converted to a full guard in the field.

Resolution:
Yes, by replacing ring nut to that of a 9001K1L style which is ring nut catalog # 9001K44 or to that of a 9001K3L style which would be 9001K111.
 
Was this helpful?
What can we do to improve the information ?