Technical FAQs

Ask a Question

What is the part number for the replacement lugs for Class 8910 Type DPA4_ definite purpose contactor?

Tang style copper lug assembly 31149-027-01. This part number does not include the lug mounting screw which can be obtained from local hardware store, TORX 10-32 x 0.375 inches.

CTA-ID : 2026725
Was this helpful?
What can we do to improve the information ?