Technical FAQs

Ask a Question

Can I get a QO120HM style high magnetic twenty amp breaker, only in a two pole version?

No. HM construction applies only to the 1 pole 15-20 A breakers. The 2 pole construction is already like the HM.

CTA-ID : 2026718
Was this helpful?
What can we do to improve the information ?