Technical FAQs

Ask a Question

Are the Horizontal Ganged Meter Sockets supplied with tenant circuit breakers or breaker mounting provisions?

Tenant circuit breakers, or provisions for them, are not provided on this product line. Separately mounted enclosed circuit breakers or safety switches should be used in conjunction with these devices.

CTA-ID : 2027026
Was this helpful?
What can we do to improve the information ?