Technical FAQs

Ask a Question

How many option cards can be used with the Altivar 58 drive?

The drive can accept one option card at a time. It is not possible to stack multiple option cars.
For example, it is not possible to have an analog I-O card and an Ethernet card on the same Altivar 58 drive.

CTA-ID : 6844
Was this helpful?
What can we do to improve the information ?