Technical FAQs

Ask a Question

Which type I-Line panels will the Powerpact J frame breakers fit into?

Issue:  
Need to know what I-line panelboards the Powerpact J-frame breaker will install into

Product line:  
Molded case circuit breakers and distribution panelboards

Environment:  
Powerpact J-frame breakers and I-line panelboards

Resolution:  
The Powerpact J frame breakers will fit into the HCM, HCP-SU, HCP and HCR-U.  Refer to Digest and Breaker Label on Panelboard.  
Was this helpful?
What can we do to improve the information ?