Technical FAQs

Ask a Question

Is the operator illuminated all the time on a 9001KR9 illuminated operator?

Button is illuminated when voltage is applied to the light module. It is separate from the push button. It can be wired to illuminate when ever the customer wants it to.


CTA-ID : 2026706
Was this helpful?
What can we do to improve the information ?