Technical FAQs

Ask a Question

Can Altivar 58 drives operate with Variable Torque and/or Constant Torque loads?

It can be used for VT or CT loads. The macro settings and other settings can be used to optimize the function of the drive to fit most VT and CT applications. CT loads typically require the drive to be de-rated when compared to the VT Amp and HP ratings. See the installation guide and the Keypad Programming manual for details.


CTA-ID : 6839
Was this helpful?
What can we do to improve the information ?