Technical FAQs

Ask a Question

Can the Altivar 58 unit use the same dynamic resistors as the ATV66, ATV16 and ATV18?

Issue: Can the Altivar 58 unit use the same dynamic resistors as the ATV66, ATV16 and ATV18?
 
Product Line: ATV58
 
Environment: All
 
Cause: N/A
 
Resolution: Yes. Actual DB resistor used depends on the application. The installation guide for the drive shows the minimum Ohms value to be used. The wattage or continuous current rating of the resistor depends on mechanical considerations.
The optional parts list shows the same DB resistor part numbers for the ATV58 as used with the ATV66.


 
Was this helpful?
What can we do to improve the information ?