Technical FAQs

Ask a Question

What type of connector is used for the Modbus connection on the VW3A58303U serial communications card?

The card has 9-pin, female SUB-D connector.
The kit includes a cable with a 15 pin SUB-D connector for connection to the Modbus network if desired. It is not necessary to use the cable.
See the MODBUS/ JBUS / UNITELWAY User?s GuideVVDED397054US Instruction Bulletin for more details.


CTA-ID : 6809
Was this helpful?
What can we do to improve the information ?