Technical FAQs

Ask a Question

Is the I-Line busway rated for 400Hz?

Our busway can be used on 400HZ systems, but must be de-rated to 85% of busway capacity.




CTA-ID : 2027013
Was this helpful?
What can we do to improve the information ?