Technical FAQs

Ask a Question

Is the EZM branch device EZML331400 available without the lever bypass and jaw release?

Issue:
Current product design

Product Line:
EZM Metering

Environment:
Product availability

Cause:
Customer request

Resolution:
The EZML331400 branch device is supplied standard with a Lever Bypass and jaw release meter sockets and CANNOT be supplied without this type of meter socket. Square D does offer a EZMK branch device which contains a K-Base BOLT-ON meter socket. BUT consult the local Utility company requirements and approval BEFORE obtaining and installing.



CTA-ID : 2027006
Was this helpful?
What can we do to improve the information ?