Technical FAQs

Ask a Question

Is the HVLcc duplex main suitable for a loop feed situation where both mains are normally closed? I can`t seem to configure it without the interlocked mains

Issue:
Is the HVLcc duplex main suitable for a loop feed situation where both mains are normally closed?  I can`t seem to configure it without the interlocked mains.

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Yes, we can omit the key interlocks for the HVL/cc duplex switches to allow both mains to be closed.


CTA-ID : 2026829
Was this helpful?
What can we do to improve the information ?