Technical FAQs

Ask a Question

Can a single pole breaker be used in the Combination Service Entrance Devices?

Issue:
Product features

Product Line:
Combination Service Entrance Device

Environment:
Branch breakers

Cause:
application

Resolution:
A single pole breaker can be used as a branch breaker in the CSEDs that contain a load center distribution section. The CSED devices that do NOT contain a load center distribution section will Only allow for the use of two pole breakers and are UL listed to be used as Service Disconnects(or main breakers).


CTA-ID : 2026484
Was this helpful?
What can we do to improve the information ?