Technical FAQs

Ask a Question

Is there a heavy duty safety switch with receptacle for a 3 pole, 4 wire application with neutral?

No. The devices has 3 hot wires and the fourth wire is connected to the switch equipment ground terminal and is not a neutral termination.

CTA-ID : 2026820
Was this helpful?
What can we do to improve the information ?