Technical FAQs

Ask a Question

Is it possible to use trench duct on the wall? Can it be mounted on a vertical surface?

Theoretically the trench duct can be mounted vertically on/in a wall but it is not recommended. The appropriate use for the trench duct is to be embedded in a concrete floor, flush with the surface of the floor.

CTA-ID : 2026694
Was this helpful?
What can we do to improve the information ?