Technical FAQs

Ask a Question

What is the standard factory jumpering on a GC200 ground fault relay?

16 jumpered to 18 when not using MDGF (Modified Differential Ground Fault) input signal, and 6 (Z3) jumpered to 7 (Z5) for ZSI (zone selective interlocking) self-restrained.

CTA-ID : 2027102
Was this helpful?
What can we do to improve the information ?