Technical FAQs

Ask a Question

Are alternate lugs available for the EZM3800CB, Series M01 Main Device?

Issue:
Need Alternate Lugs

Product Line:
EZ Meter-Pak Metering Equipment - EZM

Environment:
Alternate Lugs are needed

Cause:
Pulling nonstandard size wire

Resolution:
Standard Mechanical Lugs for an EZM3800CB, Series M01 include:
           Factory installed Main Circuit Breaker MHP36800 is supplied with the following Standard Lugs:
                  To accommodate: (3) 3/0 AWG to 500 kcmil AL/CU Wires per Phase using (1) AL900MA Lug Kit per Phase (Kit includes 1, 3-Barrel Lug)
           Line Side Neutral Assembly is supplied with the following Standard Lugs: 
                 To accommodate: (4) 3/0 AWG to 500 kcmil AL/CU Wires using (1) MMLK500 Lug Kit (Kit includes 3, 2-Barrel Lugs, only 2 of these 3 Lugs can be installed)

Alternate Mechanical Lugs:  Pulling (2) 600 kcmil AL/CU Wires per Phase and Neutral:
          Replace the (3) AL900MA Lug Kits in the MHP36800 with (3) AL800MA7 Lug Kits:
                 To accommodate: (2) 500 to 750 kcmil AL/CU Wires per Phase.
          Replace the (2) 2-Barrel Lugs on the Line Neutral with (2) 2-Barrel Lugs from Kit: MMLK250 (Kit includes 3. 2-Barrel Lugs, only 2 of these 3 Lugs can be installed) 
                 To accommodate: (2) 1/0 AWG to 600 kcmil AL/CU Wires, or (4) 1/0 AWG to 250 kcmil AL/CU Wires      

Alternate Mechanical Lugs:  Pulling (2) 750 kcmil AL/CU Wires per Phase and Neutral:
          Replace the (3) AL900MA Lug Kits in the MHP36800 with (3) AL800MA7 Lug Kits:
                 To accommodate: (2) 500 to 750 kcmil AL/CU Wires per Phase.
         Replace the (2) 2-Barrel Lugs on the Line Neutral with Lug Landing Kit EZMSK2 using 2 of the 4 Lug Pads provided.
                Lug Pads are 2" Wide with 1-3/4" Spacing between 1/2"-13 Dia. Studs. Mounting Hardware provided.
         Order (2) ILSCO Lugs TA8002N (purchased separately by other than Square D) and install them onto the Lug Pads.
               To accommodate: (2) 300 to 800 kcmil AL/CU Wires.

Alternate Mechanical Lugs: Pulling (4) 350 kcmil AL/CU Wires per Phase and Neutral
          Replace the (3) AL900MA Lug Kits in the MHP36800 with (3) AL1000MA Lug Kits:
                 To accommodate: (4) 1/0 AWG to 350 kcmil AL/CU Wires per Phase.
           The Standard Line Side Neutral Assembly is supplied with the following Lugs: 
                 To accommodate: (4) 3/0 AWG to 500 kcmil AL/CU Wires. 

Alternate Compression Lugs:  Pulling (2) 500 kcmil AL/CU Wires per Phase and Neutral
         Replace the (3) AL900MA Lug Kits in the MHP36800 with (3) VC600MA5 Lug Kits:
                To accommodate (2) 2/0 AWG to 500 kcmil AL/CU Wires per Phase
         Replace the (2) 2-Barrel Lugs on the Line Neutral with Lug Landing Kit EZMSK2 using 2 of the 4 Lug Pads provided.
                Lug Pads are 2" Wide with 1-3/4" Spacing between 1/2"-13 Dia. Studs. Mounting Hardware provided.
         Order (2) ILSCO Lugs 2ACL-500 (purchased separately by other than Square D) and install them onto the Lug Pads.
               To accommodate: (2) 4/0 AWG to 500 kcmil AL/CU Wires.

Alternate Compression Lugs:  Pulling (2) 750 kcmil AL/CU Wires per Phase and Neutral
         Replace the (3) AL900MA Lug Kits in the MHP36800 with (3) VC800MA7 Lug Kits:
                To accommodate (2) 500 to 750 kcmil AL/CU Wires per Phase
         Replace the (2) 2-Barrel Lugs on the Line Neutral with Lug Landing Kit EZMSK2 using 2 of the 4 Lug Pads provided.
                Lug Pads are 2" Wide with 1-3/4" Spacing between 1/2"-13 Dia. Studs. Mounting Hardware provided.
         Order (2) ILSCO Lugs 2IACL-750 (purchased separately by other than Square D) and install them onto the Lug Pads.
                To accommodate: (2) 500 to 750 kcmil AL/CU Wires.
                     
 
Was this helpful?
What can we do to improve the information ?