Technical FAQs

Ask a Question

What contact blocks can be used with a 9001KS88, 4 position operator, to give one contact closure per position?

Use (2) 9001KA1 blocks, one mounted on each side. The same function can be accomplished with a 9001KA2 and a 9001KA3 mounted on each side.
Was this helpful?
What can we do to improve the information ?