Technical FAQs

Ask a Question

When applying H numbers, contact assembly codes, to 9001 KX devices, what is meant by positions 1 and 2?

Looking from the back on the operator the odd positions are on the left and the even positions are on the right, starting with position 1 and 2.


CTA-ID : 2026810
Was this helpful?
What can we do to improve the information ?