Technical FAQs

Ask a Question

Can the contactor portion of a Class 8911 Type DPSO__ or Type DPSG__ starter be changed out by ordering the equivalent Class 8910 Type DPA contactor?

Issue:
Can the contactor portion of a Class 8911 Type DPSO__ or Type DPSG__ starter be changed out by ordering the equivalent Class 8910 Type DPA contactor?

Product Line:
Definite Purpose Starters

Environment:
Products sold and used in the United States

Cause:
Replacement Contacts Needed

Resolution:
Yes.


CTA-ID : 2026640
Was this helpful?
What can we do to improve the information ?