Technical FAQs

Ask a Question

What is the user manual for the digital I/O card used on the Altivar ATV58?

Bulletin VVDED397051NA describes the operation of the ALTIVAR?58 (ATV58) drive controller with the digital I/O extension card, VW3A58202, installed. This document replaces VVDED397051US R7/00 dated 7/2000.

The attachment link is to download or view the manual.

CTA-ID : 6799
Was this helpful?
What can we do to improve the information ?