Technical FAQs

Ask a Question

Where do the serial communications cards plug into the Altivar 58 drives?

Serial communications cards for the Altivar 58 drive connect directly to the main control board.
Only one option card can be connected to an ATV58 drive at a time.
Also, it is possible to communicate through the keypad port with Modbus protocol. This would not require an option card but would not allow the keypad to be connected at the same time as the network.
See the specific manual for the serial communications option in question for additional information.


CTA-ID : 6796
Was this helpful?
What can we do to improve the information ?